Feedback_Calibration_Speed
| Index.Sub | 2230.1AH |
| Data Type | Unsigned16 |
| Access | Read/Write |
| PDO Mappable |
No |
| Unit |
0.01 rpm |
|
Range |
0 to 5000 |
| Default Value | 500 |
| Store Supported | Yes |
| Description | This value is used for Closed Loop feature and defines motor speed value used during the Feedback Calibration procedure. |
|
Notes |
-- |